Responder Archive Tables

When an incident is closed or cancelled in Responder Explorer, it is added to the Responder Archive tables (assuming Archive Service is running). Use Archive Explorer to view the incidents added to the Archive tables.

Some of the fields in the Responder tables utilize domains. Domains may be edited in the ArchiveSchemaConfig.xml file.

TIP:

Information on FCID fields can be found in your geodatabase in the GDB_ITEMS and GDB_ITEMTYPES tables.

You can check the data architecture of each Responder table (i.e., field data type, field length) by viewing the SQL implementation scripts in your Miner and Miner\Responder\Developer Resources\Implementation Scripts directory.

The following table is for internal use only. Do not modify the data in this table.

  • RX_XLOCK

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.