RX_CALLS
|
Field Name |
Description |
|---|---|
|
REGION |
The region in which the call originated. This field uses the REGION domain. |
|
CRITICAL |
Indicates if the call came from a customer site that is critical. This field uses the CRITICAL_TYPE domain. |
|
HAZARD |
Indicates any hazards in the area (e.g., fire, wires down, etc.). This field uses the HAZARD domain. |
|
TROUBLE |
Indicates the problem reported by the customer (e.g., no power, flickering lights, etc.). This field uses the TROUBLE domain. |
|
DEVICE_OID |
The object ID of the device to which the customer is associated (e.g., service point or transformer). This field links to the OID field in your geodatabase. |
|
DEVICE_FCID |
The feature class ID of the device to which the customer is associated (e.g., service point or transformer). This field utilizes the DEVICE_FCID domain. |
|
INCIDENT_ID |
The ID associated with the incident resulting from the call. This field acts as a foreign key to the RX_INCIDENTS table. |
|
CUSTOMER_ACCOUNT |
The customer's account number. This field acts as a foreign key to the RX_CUSTOMERS table. |
|
CALLBACK_REQUESTED |
Indicates whether the customer requested a return call. This field uses the CALLBACK_REQUESTED domain. |
|
CALLBACK_STATUS |
Indicates whether this is a Regular Callback (0) or a Power Not Restored Callback (1). This field uses the CALLBACK_STATUS domain. |
|
TIME_RECEIVED |
The time the call was received by Responder. |
|
TIME_OUTAGE |
The time the outage occurred. |
|
TIME_RESTORED |
The time the customer's power was restored. |
|
REMARKS |
Notes from the operator or dispatcher. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
TROUBLE_AT_ACCOUNT |
Indicates whether the trouble is located at the same location as the customer's account. |
|
CAUSE |
Indicates the cause of the outage. This field uses the CAUSE domain. |
|
ANALYZING |
Indicates that a call is being analyzed. A Null value indicates the call has not been analyzed. A value of 1 indicates that a call is being analyzed. A value of 2 indicates that the call has been analyzed. All calls with an ANALYZING value of 2 should have an incident ID assigned. If not, the ANALYZING field is cleared and the call resubmitted for processing at the date/time indicated by the ANALYZING_EXPIRES_UTC field. |
|
ANALYZING_EXPIRES_UTC |
This is the coordinated universal time a call's ANALYZING and INCIDENTID fields may be cleared and the call made available for processing again. This happens only if the ANALYZING field contains a value of 1 for an extended period of time (due to contention, perhaps) or if the ANALYZING field contains a value of 2, but no incident ID has been assigned. This is a date/time field. |