RX_TAG_GROUND_STEPS_ARCHIVE

Field Name

Description

TAG_AND_GROUND_STEP_ID

A unique identifier for a tag or ground step. This field corresponds to the ID field in the RX_TAG_AND_GROUND_STEPS table.

OPERATION_ID

This field corresponds to the ID field in the RX_OPERATIONS table.

INCIDENT_ID

The ID associated with the incident associated to the tag. This field corresponds with the ID field in the RX_INCIDENTS table.

TAG_ID_1

ID of the tag.

TAG_ID_2

ID of the tag.

TAG_ID_3

ID of the tag.

TAG_TYPE

The type of tag placed.

PHASES

Indicates which phases are affected.

ACTION

Indicates whether the action is a place or remove.

TAG_GUID

The ID associated with the incident associated with the tag. This field corresponds with the ID field in the RX_INCIDENTS table.

USER_CREATED

The name of the user who created the record. This field is populated automatically by Responder.

USER_UPDATED

The name of the user who updated the record. This field is populated automatically by Responder.

CHANGE_DATE

The time and date an operation was performed on the record.

OPERATION

The operation (e.g., insert, delete, update) performed on the record.

USER_UPDATED_ARCH

This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record.

GROUND

Indicates whether the step is a ground (yes/no).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?