RX_TAG_GROUND_STEPS_HISTORY
Field Name |
Description |
---|---|
TAG_AND_GROUND_STEP_ID |
A unique identifier for a tag or ground step. This field corresponds to the ID field in the RX_TAG_AND_GROUND_STEPS table. |
TAG_ID_1 |
ID of the tag. |
TAG_ID_2 |
ID of the tag. |
TAG_ID_3 |
ID of the tag. |
OPERATION_ID |
This field corresponds to the ID field in the RX_OPERATIONS table. |
TAG_TYPE |
The type of tag placed. |
PHASES |
Indicates which phases are affected. |
ACTION |
Indicates whether the action is a place or remove. |
GROUND |
Indicates whether the step is a ground (yes/no). |
USER_CREATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who created the record. |
USER_UPDATED |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
CHANGE_DATE |
The date an operation was performed on the incident record. |
OPERATION |
The operation (e.g., insert, delete, update) performed on the incident record. |
TAG_GUID |
The GUID assigned to the tag. |