RX_INCIDENT_CAUSE_STATISTICS_ARCHIVE

Field Name

Description

CAUSE

Indicates the cause of the outage. This field uses the CAUSE domain.

CAUSE_DESCRIPTION

A description of the type of event that caused the incident.

SAIDI

Stands for System Average Interruption Duration Index, this field reports the average length of time customers were without power for the incident.

DURATION_SUM

The sum of durations all customers were without power.

CUSTOMER_SERVED

Total number of customers served.

OUTAGE_COUNT

Number of distinct customer outages.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.