Line Display Services Configuration
Once you configured the Line Display Services configuration file (Miner.Responder.LineDisplayService.exe.config), you must start the Line Display Services. The Line Display Services must remain active to run Responder Line Display.
The Count field indicates the number of Line Display Services running. Since only one Line Display Services can be run per organization, the count should be one. If you change this value to 0 and click Apply, the Arguments field becomes enabled. Use this field to set your geodatabase server along with any arguments.
To start Line Display Services, type the number one in the Count field and click Apply. When Line Display Services are running, you may not edit the Arguments field. The Path field always remains disabled. This field provides the path to the executable that launches Line Display Services.