RX_GLOBALID_XREF
This table is used only when you have implemented the optional Esri replication support. In order to support Esri replication, Responder requires this table to help manage GUIDs.
|
Field Name |
Description |
|---|---|
|
FCID |
The feature class ID of the feature impacted by an incident. |
|
OID |
The object ID of the feature impacted by an incident. |
|
GLOBALID |
The GlobalID (GUID) of the feature impacted by an incident. |
|
FCID_ACTUAL |
Currently not used by Responder. This field should contain the FCID of the feature as it appears in the replicated database. |
|
OID_ACTUAL |
Currently not used by Responder. This field should contain the OID of the feature as it appears in the replicated database. |