RX_INCIDENT_FEATURES
|
Field Name |
Description |
|---|---|
|
OID |
Object ID of the feature associated with the incident. |
|
FCID |
Feature class ID of the feature associated with the incident. |
|
SUBID |
The unique ID of each segment of a complex edge. |
|
X |
The x-coordinate of the incident feature. |
|
Y |
The y-coordinate of the incident feature. |
|
INCIDENT_ID |
The ID associated with the incident. This field acts as a foreign key to the RX_INCIDENTS table. |
|
TIME_REPORTED |
Time that the feature was reported out. |
|
CONFIRMED |
Indicates whether the feature has been confirmed out. This field uses the CONFIRMED domain. |
|
FACILITY_ID |
The Facility ID of the incident feature as defined in the geodatabase. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
REMARKS |
Notes from the operator or dispatcher. |
|
REGION |
The region in which the device resides. This field uses the REGION domain. |
|
CANCEL_REASON |
Reason the feature was cancelled. |