Addon Scripts - Oracle
Addon scripts are available to support optional Responder configurations. By default, these scripts are installed here: \Program Files\Miner and Miner\Responder\Developer Resources\Implementation Scripts\Oracle\Addons.
Execute only the scripts for the optional functionality to implement.
Esri Replication
Replication_oracle.sql: This script provides the tables necessary to support GlobalIDs and Esri Replication. The script name may be preceded by the current release version (e.g., 930_Replication_oracle.sql).
This script adds the following table (assign correct permissions):
RX_GLOBALID_XREF
Telemetry
Telemetry.sql: This script sets up the tables and fields required to implement the Telemetry service. The script name may be preceded by the current release version (e.g., 1003_Telemetry_oracle.sql).
This script adds the following table (assign correct permissions):
RX_TELEMETRY