RX_CREW_SUB_ASSIGNMENTS_ARCHIVE
|
Field Name |
Description |
|
SUB_ASSIGNMENT_ID |
Internal database field used as foreign key during crew assignment. |
|
INCIDENT_ID |
The ID associated with the incident resulting from the call. This field corresponds with the ID field in the RX_INCIDENTS table. |
|
CREW_ARCHIVE_ID |
Crew ID when archived. |
|
CREW_NAME |
The name of the crew. |
|
INCIDENT_CHILD_TYPE |
The type of feature to which the crew record was associated. |
|
FCID |
Feature class ID of the feature. |
|
OID |
Object ID of the feature |
|
FACILITY_ID |
The Facility ID of the incident feature as defined in the geodatabase. |
|
CHANGE_DATE |
The time and date an operation was performed on the record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |