RX_T_MAJOR_EVENT_DAY
The Calculate Tmed tool (in Archive Explorer) calculates the Major Event Duration (med) according to the IEEE Standard 1366-2012, section 4.5. When these values are calculated, they are stored in this table. Any incident that has a duration which exceeds the TMED_MINUTES value will be excluded from the Reliability Reports.
|
Field Name |
Description |
|
START_DATE |
The outage date (Time of Outage field) of the first load point archive record within the five-year period. |
|
END_DATE |
The outage date (Time of Outage field) of the last load point archive record within the five-year period. |
|
TMED_MINUTES |
The length of the major event duration (med). |