RX_TRUCKS_ARCHIVE
|
Field Name |
Description |
|---|---|
|
TRUCK_ID |
The unique identifier assigned to the truck. This field corresponds to the ID field in the RX_TRUCKS table. |
|
ASSIGNMENT_ID |
The unique identifier assigned to each crew assignment. This field corresponds with the ID field in the RX_CREW_ASSIGNMENTS table. |
|
NUMBER |
The number assigned to the truck as an identifier. |
|
REGION |
The region in which the truck is located. This field uses the REGION domain. |
|
TRUCK_TYPE |
The type of truck. |
|
RADIO1 |
The radio frequency at which the crew can be reached. |
|
RADIO2 |
An alternative radio frequency at which the crew can be reached. |
|
COMPANY |
The company to which the truck belongs. This field uses the COMPANY domain. |
|
STATUS |
The status of the truck. This field uses the STATUS domain. |
|
CREW_ID |
Indicates the ID for the crew to which the truck has been assigned. This field corresponds to the ID field in the RX_CREWS table. |
|
USER_CREATED |
The name of the user who created the record. This field is populated automatically by Responder. |
|
USER_UPDATED |
The name of the user who updated the record. This field is populated automatically by Responder. |
|
CHANGE_DATE |
The time and date an operation was performed on the record. |
|
OPERATION |
The operation (e.g., insert, delete, update) performed on the record. |
|
USER_UPDATED_ARCH |
This field is not currently used by Responder. You may customize Responder to populate this field with the name of the user who updated the record. |
|
INCIDENT_ID |
The ID associated with the incident. This field acts as a foreign key to the RX_INCIDENTS table. |