QGH1336306-06

状态输入 (DI) 应用(适用于 PM1140H)

状态输入用于监控外部触点或电路断路器的状态。

测量仪的状态输入需要使用外部电压源或湿性电压(在测量仪中提供)来探测状态输入的“开/关”状态。如果状态输入的外部电压在运行范围内,则测量仪处于打开状态。

状态输入接线

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

这有帮助吗?