Device Internal Error Logs
Description
The last 20 device internal errors are recorded by the LTMT main unit. Each detected internal error log is composed of 8 registers.
A read request of 8xn registers is necessary to read n detected internal error logs, where 8 is the number of registers for each detected internal error log.
The order and the description of the registers for detected internal error log 1 are valid for the other detected internal error logs.
| Address | Register | Description |
|---|---|---|
| 0x1F40–0x1F47 | 8001–8008 |
Detected internal error log 1 (most recent log) |
| ... | ... | ... |
| 0x1F40–0x1F47 | 8001+8x(n-1) – 8008+8x(n-1) | Detected internal error log n |
| ... | ... | ... |
| 0x1FD8–0x1FDF | 8153–8160 | Detected internal error log 20 |
Device Internal Error Log 1 Registers
The table lists the registers for the detected internal error log 1.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
| 0x1F40 | 8001 | 4 |
0x03 |
R |
– |
– |
UINT16 |
Y | |
| 0x1F44 | 8005 | 1 |
0x03 |
R |
– |
– |
UINT16 |
Y | Detected Internal Error Code |
| 0x1F45 | 8006 | 3 |
0x03 |
R |
– |
– |
UINT16 |
Y | Reserved |