DOCA0355EN-01

Measured Ground Trip

The table lists the measured ground trip for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DE7

3560

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm
  • 2: Trip
  • 3: Alarm and Trip

0

Y

Function setting

0x0DE8

3561

1

0x03,
0x06,
0x10

RW

1

mA

UINT16

20–20000
(step 10)

30

Y

Pickup

0x0DE9

3562

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

1

Y

Time delay

0x0DEA

3563

1

0x03,
0x06,
0x10

RW

1

mA

UINT16

20–20000
(step 10)

30

Y

Alarm level

0x0DEB

3564

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0DEC

3565

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0DED

3566

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Enable

0

N

Function while motor starting

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?