DOCA0355EN-01

Digital Input Status

The table lists the digital input status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0000

1

0x02

R

BOOL

N

Digital input 1 

0x0001

2

0x02

R

BOOL

N

Digital input 2

0x0002

3

0x02

R

BOOL

N

Digital input 3

0x0003

4

0x02

R

BOOL

N

Digital input 4

0x0004

5

0x02

R

BOOL

N

Digital input 5

0x0005

6

0x02

R

BOOL

N

Digital input 6

0x0006

7

0x02

R

BOOL

N

Digital input 7

0x0007

8

0x02

R

BOOL

N

Digital input 8

0x0008

9

0x02

R

BOOL

N

Digital input 9

0x0009

10

0x02

R

BOOL

N

Digital input 10

0x000A

11

0x02

R

BOOL

N

Digital input 11

0x000B

12

0x02

R

BOOL

N

Digital input 12

0x000C

13

0x02

R

BOOL

N

Digital input 13

0x000D

14

0x02

R

BOOL

N

Digital input 14

0x000E

15

0x02

R

BOOL

N

Digital input 15

0x000F

16

0x02

R

BOOL

N

Digital input 16

0x0010

17

0x02

R

BOOL

N

Digital input 17

0x0011

18

0x02

R

BOOL

N

Digital input 18

0x0012

19

0x02

R

BOOL

N

Digital input 19

0x0013

20

0x02

R

BOOL

N

Digital input 20

0x0014

21

0x02

R

BOOL

N

Digital input 21

0x0015

22

0x02

R

BOOL

N

Digital input 22

0x0016

23

0x02

R

BOOL

N

Digital input 23

0x0017

24

0x02

R

BOOL

N

Digital input 24

0x0018–0x001F

25–32

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?