Voltage Dip
The table lists the voltage dip for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0EAD |
3758 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
| 0x0EAE |
3759 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%Vn |
UINT16 |
20–90 |
90 |
Y |
Voltage dip |
| 0x0EAF |
3760 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%Vn |
UINT16 |
20–95 |
95 |
Y |
Voltage restoration |
|
0x0EB0 |
3761 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
s |
UINT16 |
0–9999 |
2 |
Y |
Voltage dip restart timeout |
|
0x0EB1 |
3762 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
s |
UINT16 |
0–301 |
4 |
Y |
Delayed restart timeout |
|
0x0EB2 |
3763 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Bypass STOP DI |
|
0x0EB3 |
3764 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–4 |
2 |
Y |
Immediate restart timeout |
|
0x0EB4 |
3765 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
s |
UINT16 |
1–9999 |
10 |
Y |
Load shedding timeout |
|
0x0EB5 |
3766 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |