Current Phase Loss Protection
The table lists the current phase loss protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0DFD |
3582 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
|
0x0DFE |
3583 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
|
0x0DFF |
3584 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E00 |
3585 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E01 |
3586 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |