Phase Under Voltage Protection
The table lists the phase under voltage protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0E29 |
3626 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
|
0x0E2A |
3627 |
1 |
0x03, |
RW |
1 |
%Vn |
UINT16 |
20–100 |
80 |
Y |
Pickup |
|
0x0E2B |
3628 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
1–60000 |
100 |
Y |
Time delay |
|
0x0E2C |
3629 |
1 |
0x03, |
RW |
1 |
%Vn |
UINT16 |
20–100 |
80 |
Y |
Alarm level |
|
0x0E2D |
3630 |
1 |
0x03, |
RW |
1 |
– |
BITMAP |
|
8 |
Y |
Reset mode |
|
0x0E2E |
3631 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E2F |
3632 |
2 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |