Over Frequency Protection
The table lists the over frequency protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0E50 |
3665 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0E51 |
3666 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%F* |
UINT16 |
100–110 |
105 |
Y |
Pickup |
|
0x0E52 |
3667 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
|
0x0E53 |
3668 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%F* |
UINT16 |
100–110 |
105 |
Y |
Alarm level |
|
0x0E54 |
3669 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E55 |
3670 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E56 |
3671 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |