DOCA0355EN-01

Function Codes

The TeSys Tera system supports the following Modbus RTU function codes:

Function Code

Description

2 (0x02)

Read discrete inputs

3 (0x03)

Read holding registers

4 (0x04)

Read input registers

6 (0x06)

Write single holding register

16 (0x10)

Write multiple holding registers

23 (0x17)

Read or Write multiple holding registers

43 or 14 (0x2B or 0x0E)

Read device identification

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?