Inhibit Status
The table lists the inhibit status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
| 0x0240 |
577 |
0x02 |
R |
BOOL | N |
No voltage inhibit |
| 0x0241 |
578 |
0x02 |
R |
BOOL | N |
Under voltage inhibit |
| 0x0242 |
579 |
0x02 |
R |
BOOL | N |
Trip inhibit |
| 0x0243 |
580 |
0x02 |
R |
BOOL | N |
Thermal inhibit |
| 0x0244 |
581 |
0x02 |
R |
BOOL | N |
Max starts inhibit |
| 0x0245 |
582 |
0x02 |
R |
BOOL | N |
Interlock 1 inhibit |
| 0x0246 |
583 |
0x02 |
R |
BOOL | N |
Interlock 2 inhibit |
| 0x0247 |
584 |
0x02 |
R |
BOOL | N |
Interlock 3 inhibit |
| 0x0248 |
585 |
0x02 |
R |
BOOL | N |
Interlock 4 inhibit |
| 0x0249 |
586 |
0x02 |
R |
BOOL | N |
Interlock 5 inhibit |
| 0x024A |
587 |
0x02 |
R |
BOOL | N |
Interlock 6 inhibit |
| 0x024B |
588 |
0x02 |
R |
BOOL | N |
Interlock 7 inhibit |
| 0x024C |
589 |
0x02 |
R |
BOOL | N |
Interlock 8 inhibit |
| 0x024D |
590 |
0x02 |
R |
BOOL | N |
Interlock 9 inhibit |
| 0x024E |
591 |
0x02 |
R |
BOOL | N |
Interlock 10 inhibit |
| 0x024F |
592 |
0x02 |
R |
BOOL | N |
Interlock 11 inhibit |
| 0x0250 |
593 |
0x02 |
R |
BOOL | N |
Interlock 12 inhibit |
| 0x0251 |
594 |
0x02 |
R |
BOOL | N |
Local DI stop inhibit |
| 0x0252 |
595 |
0x02 |
R |
BOOL | N |
Remote DI stop inhibit |
| 0x0253 |
596 |
0x02 |
R |
BOOL | N |
Communication stop inhibit |
| 0x0254 |
597 |
0x02 |
R |
BOOL | N |
Force stop inhibit |
| 0x0255 |
598 |
0x02 |
R |
BOOL | N |
Antibackspin inhibit |
| 0x0257 |
600 |
0x02 |
R |
BOOL | N |
Direction change inhibit |
| 0x0258 |
601 |
0x02 |
R |
BOOL | N |
Speed change inhibit |
| 0x0259 |
602 |
0x02 |
R |
BOOL | N |
Custom stop inhibit |
| 0x025A |
603 |
0x02 |
R |
BOOL | N |
Firmware update inhibit |
| 0x025B–0x025F |
604–608 |
0x02 |
R |
BOOL | N |
Reserved |