DOCA0355EN-01

Phase Over Voltage Protection

The table lists the phase over voltage protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E31

3634

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

2

Y

Function setting

0x0E32

3635

1

0x03,
0x06,
0x10

RW

1

%Vn

UINT16

101–130
(step 1)

110

Y

Pickup

0x0E33

3636

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

50

Y

Time delay

0x0E34

3637

1

0x03,
0x06,
0x10

RW

1

%Vn

UINT16

101–130
(step 1)

110

Y

Alarm level

0x0E35

3638

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0E36

3639

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E37

3640

1

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?