Calculated Ground Trip
The table lists the calculated ground trip for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0DE0 |
3553 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
2 |
Y |
Function setting |
|
0x0DE1 |
3554 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
10–500 |
20 |
Y |
Pickup |
|
0x0DE2 |
3555 |
1 |
0x03, 0x06, 0x10 |
RW |
0.010–10 |
s |
UINT16 |
5–60000 |
20 |
Y |
Time delay |
|
0x0DE3 |
3556 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
10–500 |
20 |
Y |
Alarm level |
|
0x0DE4 |
3557 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0DE5 |
3558 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0DE6 |
3559 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
N |
Function while motor starting |