DOCA0355EN-01

Analog Module Data

The table lists the analog module data for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Svd

Description

0x15D1

5586

1

0x03

R

0.1

mA

INT16

N

Analog input 1

0x15D2

5587

1

0x03

R

0.1

mA

INT16

N

Analog input 2

0x15D3

5588

1

0x03

R

0.1

mA

INT16

N

Analog input 3

0x15D4

5589

1

0x03

R

0.1

mA

INT16

N

Analog input 4

0x15D5

5590

4

Reserved

0x15D9

5594

1

0x03

R

0.1

mA

INT16

N

Analog output 1

0x15DA

5595

1

0x03

R

0.1

mA

INT16

N

Analog output 2

0x15DB

5596

2

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?