Starter Settings
The table lists the starter settings for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X | Unit |
Type |
Range | Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x1144 |
4421 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
0: Motor 1: Heater |
0 |
Y |
Load type |
|
0x1145 |
4422 |
1 |
0x03, 0x06 ,0x10 |
RW |
1 |
– |
UINT16 |
0–10 (step 1) |
1 |
Y |
|
|
0x1146 |
4423 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
0: Disable 1: HMI 2: DI 3: Communication |
0 |
Y |
Mode selection |
|
0x1147 |
4424 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
Bit 0: HMI Bit 1: Local DI Bit 2: Remote DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Local 1 start source |
|
0x1148 |
4425 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
Bit 0: HMI Bit 1: Local DI Bit 2: Remote DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Local 2 start source |
|
0x1149 |
4426 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
Bit 0: HMI Bit 1: Local DI Bit 2: Remote DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Local 3 start source |
|
0x114A |
4427 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
Bit 0: HMI Bit 1: Local DI Bit 2: Remote DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Remote start source |
|
0x114B |
4428 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
Bit 0: HMI Bit 1: Local DI Bit 2: Remote DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Local 1 stop source |
|
0x114C |
4429 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
Bit 0: HMI Bit 1: Local DI Bit 2: Remote DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Local 2 stop source |
|
0x114D |
4430 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
Bit 0: HMI Bit 1: Local DI Bit 2: Remote DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Local 3 stop source |
|
0x114E |
4431 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
Bit 0: HMI Bit 1: Local DI Bit 2: Remote DI Bit 3: Communication Bit 4: Custom logic |
11 |
Y |
Remote stop source |
|
0x114F |
4432 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
0: Momentary 1: Maintained |
0 |
Y |
Local DI start input |
|
0x1150 |
4433 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
0: Momentary 1: Maintained |
0 |
Y |
Remote DI start input |
|
0x1151 |
4434 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
0: Momentary 1: Maintained |
0 |
Y |
Custom start input |
|
0x1152 |
4435 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
0: Bump 1: Bumpless |
0 |
N |
Mode transfer |
|
0x1153 |
4436 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
0: Momentary 1: Maintained |
0 |
Y |
Communication start input |
|
0x1154–0x1155 |
4437–4438 |
3 |
– | – | – | – | – | – | – | – |
Reserved |
|
0x1156 |
4439 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
0: Disable 1: Enable |
0 |
Y |
Change direction |
|
0x1157 |
4440 |
1 |
0x03, 0x06, 0x10 |
RW |
0.01 |
s |
UINT16 |
1–60000 (step 1) |
50 |
Y |
Feedback response time |
|
0x1158 |
4441 |
1 |
0x03, 0x06, 0x10 |
RW |
0.01 |
s |
UINT16 |
1–60000 (step 1) |
50 |
Y |
Motor current sensing time |
|
0x1159 |
4442 |
1 |
0x03, 0x06, 0x10 |
RW |
0.01 |
s |
UINT16 |
1–60000 (step 1) |
6000 |
Y |
Interlocking time |
|
0x115E–0x1160 |
4443–4449 |
3 |
– | – | – | – | – | – | – | – |
Reserved |
|
0x1161 |
4450 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
0: Three phase 1: Single phase |
0 |
Y |
Number of phases |
| 0x1162 |
4451 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
0: DI+Current based 1: Current based |
1 |
Y |
Stop detection |
| 0x1163 |
4452 |
1 |
0x03, 0x06, 0x10 |
RW |
1 | – |
UINT16 |
0: Disable 1: Enable |
0 |
Y |
Forced start function |
Starter Type
The table lists the type of starters and the time delays related to the starter types.
| Starter type |
Value |
Delay 1 | Delay 2 | Delay 3 | Delay 4 |
|---|---|---|---|---|---|
| Direct online |
1 |
– | – | – | – |
|
Reverse direct online * |
2 |
– | – | – | – |
| Star delta |
3 |
Time in star | Change over time | – | – |
| Overload |
0 |
– | – | – | – |