Analog Protection Status
Analog Protection Alarm Status
The table lists the analog protection alarm status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
|
0x0190 |
401 |
0x02 |
R |
BOOL | N |
AI1 alarm |
|
0x0191 |
402 |
0x02 |
R |
BOOL | N |
AI2 alarm |
|
0x0192 |
403 |
0x02 |
R |
BOOL | N |
AI3 alarm |
|
0x0193 |
404 |
0x02 |
R |
BOOL | N |
AI4 alarm |
|
0x0194–0x019F |
405–416 |
– |
– |
– |
– |
Reserved |
Analog Protection Pickup Status
The table lists the analog protection pickup status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
|
0x01A0 |
417 |
0x02 |
R |
BOOL | N |
AI1 pickup |
|
0x01A1 |
418 |
0x02 |
R |
BOOL | N |
AI2 pickup |
|
0x01A2 |
419 |
0x02 |
R |
BOOL | N |
AI3 pickup |
|
0x01A3 |
420 |
0x02 |
R |
BOOL | N |
AI4 pickup |
|
0x01A4–0x01AF |
421–432 |
– |
– |
– |
– |
Reserved |
Analog Protection Trip Status
The table lists the analog protection trip status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
|
0x01B0 |
433 |
0x02 |
R |
BOOL | N |
AI1 trip |
|
0x01B1 |
434 |
0x02 |
R |
BOOL | N |
AI2 trip |
|
0x01B2 |
435 |
0x02 |
R |
BOOL | N |
AI3 trip |
|
0x01B3 |
436 |
0x02 |
R |
BOOL | N |
AI4 trip |
|
0x01B4–0x01BF |
437–448 |
– |
– |
– |
– |
Reserved |