Digital Input Settings
Description
The TeSys Tera system supports maximum 32 digital inputs:
- Four digital inputs on the LTMT main unit.
- Up to 28 digital inputs with LTMT expansion modules.
| Address | Register | No. | Description | DI location |
|---|---|---|---|---|
|
0x1194 |
4501 |
3 |
Digital input 1 settings |
DI1 on LTMT main unit |
|
0x1197 |
4504 |
3 |
Digital input 2 settings |
DI2 on LTMT main unit |
|
0x119A |
4507 |
3 |
Digital input 3 settings |
DI3 on LTMT main unit |
|
0x119D |
4510 |
3 |
Digital input 4 settings |
DI4 on LTMT main unit |
|
0x11A0 |
4513 |
3 |
Digital input 5 settings |
DI on LTMT expansion module |
|
0x11A3 |
4516 |
3 |
Digital input 6 settings |
DI on LTMT expansion module |
|
0x11A6 |
4519 |
3 |
Digital input 7 settings |
DI on LTMT expansion module |
|
0x11A9 |
4522 |
3 |
Digital input 8 settings |
DI on LTMT expansion module |
|
0x11AC |
4525 |
3 |
Digital input 9 settings |
DI on LTMT expansion module |
|
0x11AF |
4528 |
3 |
Digital input 10 settings |
DI on LTMT expansion module |
|
0x11B2 |
4531 |
3 |
Digital input 11 settings |
DI on LTMT expansion module |
|
0x11B5 |
4534 |
3 |
Digital input 12 settings |
DI on LTMT expansion module |
|
0x11B8 |
4537 |
3 |
Digital input 13 settings |
DI on LTMT expansion module |
|
0x11BB |
4540 |
3 |
Digital input 14 settings |
DI on LTMT expansion module |
|
0x11BE |
4543 |
3 |
Digital input 15 settings |
DI on LTMT expansion module |
|
0x11C1 |
4546 |
3 |
Digital input 16 settings |
DI on LTMT expansion module |
|
0x11C4 |
4549 |
3 |
Digital input 17 settings |
DI on LTMT expansion module |
|
0x11C7 |
4552 |
3 |
Digital input 18 settings |
DI on LTMT expansion module |
|
0x11CA |
4555 |
3 |
Digital input 19 settings |
DI on LTMT expansion module |
|
0x11CD |
4558 |
3 |
Digital input 20 settings |
DI on LTMT expansion module |
|
0x11D0 |
4561 |
3 |
Digital input 21 settings |
DI on LTMT expansion module |
|
0x11D3 |
4564 |
3 |
Digital input 22 settings |
DI on LTMT expansion module |
|
0x11D6 |
4567 |
3 |
Digital input 23 settings |
DI on LTMT expansion module |
|
0x11D9 |
4570 |
3 |
Digital input 24 settings |
DI on LTMT expansion module |
|
0x11DC–0x11F1 |
4573–4594 |
3 |
– |
Reserved |
The settings of the four digital inputs on the LTMT main unit corresponds to the settings of digital input 1 to digital input 4.
The settings of digital inputs on a LTMT expansion module are defined according to the expansion unit configuration.
Example: If the TeSys Tera system is composed of:
-
One LTMT main unit.
-
One LTMTIN42 BD/FM expansion unit with four digital inputs, configured as expansion unit 1.
Then,
- Digital input 1 settings to Digital input 4 settings are valid for DI1 to DI4 on the LTMT main unit.
-
Digital input 5 settings to Digital input 8 settings are valid for DI5 to DI8 on the LTMTIN42 expansion unit.
Digital Input 1 Settings
The table lists the registers for the digital input settings.
|
Address |
Register |
No. |
Function code |
RW |
X | Unit |
Type |
Range | Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
| 0x1194 | 4501 | 1 |
0x03, |
RW |
1 |
– |
UINT16 |
0: Active high 1: Active low |
0 |
Y |
Digital input 1 trigger type |
| 0x1195 | 4502 | 1 |
0x03, |
RW |
1 |
– |
UINT16 |
0–38 |
4 |
Y |
Digital input 1 input source |
| 0x1196 | 4503 | 1 |
0x03, |
RW |
1 | ms | UINT16 |
1–60000 |
10 |
Y |
Digital input 1 validation time |
DI Input Source
The table lists the input source for the digital input settings.
| Register value | DI input source |
|---|---|
|
0 |
Other |
|
1 |
Trip Reset DI |
|
2 |
Breaker Close DI |
|
3 |
Breaker Open DI |
|
4 |
Local-START> DI |
|
5 |
Local-START>> DI |
|
6 |
Local-STOP DI |
|
7 |
Local-START< DI |
|
8 |
Local-START<< DI |
|
9 |
Remote-START> DI |
|
10 |
Remote-START>> DI |
|
11 |
Remote-STOP DI |
|
12 |
Remote-START< DI |
|
13 |
Remote-START<< DI |
|
14 |
Interlock 1 |
|
15 |
Interlock 2 |
|
16 |
Interlock 3 |
|
17 |
Interlock 4 |
|
18 |
Interlock 5 |
|
19 |
Interlock 6 |
|
20 |
Interlock 7 |
|
21 |
Interlock 8 |
|
22 |
Interlock 9 |
|
23 |
Interlock 10 |
|
24 |
Interlock 11 |
|
25 |
Interlock 12 |
|
26 |
Contactor Open DI |
|
27 |
Run DI |
|
28 |
Block Input |
|
29 |
Logic Test DI |
|
30 |
Mode Selection 1 |
|
31 |
Mode Selection 2 |
|
32 |
Speed Change |
|
33 |
Forced Start |
|
34 |
Forced Stop |
|
35 |
Self Test without Trip |
|
36 |
Self Test with Trip |
|
37 |
Reserved |
|
38 |
None |