Modbus RTU HMI Connection Port
The HMI port on LTMT main unit with Modbus RTU protocol can also be used as an optional Modbus RTU communication port.
When the LTMT HMI port is used as Modbus RTU communication port:
-
LTMT main unit is connected to a Modbus RTU client in a point-to-point connection.
-
Modbus RTU client can be connected to the HMI port.
-
HMI port can be connected temporarily to a PC running the TeSys Tera DTM embedded in a FDT container for TeSys Tera system configuration.
The HMI port characteristics are:
| Physical interface | RS 485 wire |
| Connector | RJ45 |
Connection Diagram
A Modbus RTU client can be connected to the HMI port on the front face of the LTMT main unit, as shown in the diagram below.
| A | Modbus RTU client (PC or PLC) |
| B | Modbus RTU cable |
| C | LTMT main unit |
Modbus RTU Cables
The table lists the Modbus RTU cables used for connection.
|
Designation |
Length |
|---|---|
|
Shielded cable for Modbus RTU bus, with two RJ45 connectors |
0.3 m (1 ft) |
|
1 m (3.2 ft) |
|
|
3 m (9.8 ft) |
|
| Connection cable USB or RJ45 | 2.5 m (8.20 ft) |
LTMT HMI Port Pinout
The LTMT main unit is connected to the Modbus RTU network with a shielded RJ45 connector in compliance with the following wiring:
|
Pin No. |
Signal |
Description |
|---|---|---|
|
1 |
– |
Not connected |
|
2 |
– |
Not connected |
|
3 |
– |
Not connected |
|
4 |
D1 or D(B) |
Transceiver terminal 1 |
|
5 |
D0 or D(A) |
Transceiver terminal 0 |
|
6 |
– |
Not connected |
|
7 |
+5V |
Auxiliary supply to HMI |
|
8 |
0VL |
Signal and power supply common |
LTMT HMI Port Settings
The LTMT HMI port has the following configurable settings:
| Setting | Setting range | Default setting |
|---|---|---|
| Node address | 1–247 in step of 1 | 1 |
| Parity |
|
Even |
| Baud rate |
|
19200 bps |
|
Endianness |
|
Big-endian |
-
Node address: 1
-
Baud rate: 19200 bps
-
Parity: Even
-
Endianness: Big-endian
The LTMT HMI port settings can be configured using the following interfaces:
-
A PC running the TeSys Tera DTM embedded in a FDT container, such as SoMove software.
-
A PLC or DCS through the communication protocol.