DOCA0355EN-01

Starter Commands

The table lists the starter commands for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x01F0

497

0x02

R

BOOL N

Contactor output 1

0x01F1

498

0x02

R

BOOL N

Contactor output 2

0x01F2

499

0x02

R

BOOL N

Contactor output 3

0x01F3

500

0x02

R

BOOL N

Contactor output 4

0x01F4

501

0x02

R

BOOL N

Contactor output 5

0x01F5–0x020E

502–527

Reserved

0x020F 528

0x02

R

BOOL N Motor Stop
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?