DOCA0355EN-01

Voltage Imbalance Protection

The table lists the voltage imbalance protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0E3D

3646

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

3

Y

Function setting

0x0E3E

3647

1

0x03,
0x06,
0x10

RW

1

%Vn

UINT16

5–50
(step 5)

10

Y

Pickup

0x0E3F

3648

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

100

Y

Time delay

0x0E40

3649

1

0x03,
0x06,
0x10

RW

1

UINT16

5–50
(step 5)

10

N

Alarm level

0x0E41

3650

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0E42

3651

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0E43

3652

1

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?