Excessive Start Time Protection
The table lists the excessive start time protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0EA6 |
3751 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0EA7 |
3752 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
100 |
Y |
Time delay |
|
0x0EA8 |
3753 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0EA9 |
3754 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0EAA |
3755 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
80–300 |
100 |
Y |
Run Threshold |
|
0x0EAB–0x0EAC |
3756–3757 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |