System Settings
The table lists the system settings for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X | Unit |
Type |
Range | Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x1164 |
4453 |
1 |
0x03, 0x10 |
RW |
1 |
A |
UINT16 |
1–1000 (step 1) |
1 |
Y |
Phase CT primary |
|
0x1165 |
4454 |
1 |
0x03, 0x10 |
RW |
1 |
A |
UINT16 |
1–5 (step 4) |
1 |
Y |
Phase CT secondary |
|
0x1166 |
4455 |
2 |
– | – | – | – | – | – | – | – |
Reserved |
|
0x1168 |
4457 |
1 |
0x03, 0x10 |
RW |
1 |
A |
UINT16 |
1–1000 (step 1) |
1 |
Y |
Speed 2 CT primary |
|
0x1169 |
4458 |
1 |
0x03, 0x10 |
RW |
1 |
A |
UINT16 |
1–5 (step 4) |
1 |
Y |
Speed 2 CT secondary |
|
0x116A–0x116C |
4459–4461 |
3 |
– | – | – | – | – | – | – | – |
Reserved |
|
0x116D |
4462 |
1 |
0x03, 0x10 |
RW |
0.1 |
V |
UINT16 |
1100–6900 (step 1) |
4150 |
Y |
Nominal voltage (Vn) |
|
0x116E |
4463 |
1 |
0x03, 0x10 |
RW |
1 |
– |
UINT16 |
0: 50Hz 1: 60Hz |
0 |
Y |
Nominal frequency (Fn) |
|
0x116F |
4464 |
1 |
0x03, 0x10 |
RW |
1 |
– |
UINT16 |
0: L123 1: L132 |
0 |
Y |
Phase rotation |
|
0x1170 |
4465 |
1 |
0x03, 0x10 |
RW |
1 |
– |
UINT16 |
0: Disable 1: Enable |
1 |
Y |
Voltage input* |
|
0x1171 |
4466 |
1 | – | – | – | – | – | – | – | – |
Reserved |
|
0x1172 |
4467 |
1 |
0x03, 0x10 |
RW |
0.1 |
A |
UINT16 |
1–10000 (step 1) |
25 |
Y |
Full load current (FLC1) |
|
0x1173 |
4468 |
1 |
0x03, 0x10 |
RW |
0.1 |
A |
UINT16 |
1–10000 (step 1) |
25 |
Y |
Speed 2 full load current (FLC2) |
|
0x1174 |
4469 |
1 | 0x03, 0x10 |
RW |
0 |
– |
UINT16 |
1–10 (step 1) |
1 | N | Phase CT secondary passes |
|
0x1175 |
4470 |
1 | 0x03, 0x10 |
RW |
1 |
– |
UINT16 |
1–10 (step 1) |
1 | N | Speed 2 phase secondary passes |
| 0x1176 |
4471 |
3 |
– | – | – | – | – | – | – | – |
Reserved |
| 0x1179 |
4474 |
1 |
0x03, 0x10 |
RW |
1 |
– |
UINT16 |
0: Disable 1: Enable |
1 |
Y |
Test mode |
| 0x117A |
4475 |
1 |
0x03, 0x10 |
RW |
1 |
– |
UINT16 |
0: No 1: Yes |
0 |
Y |
Bypass interlocks during test |