Anti-Backspin Timer
The table lists the anti-backspin timer for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0EDA |
3803 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0EDB |
3804 |
1 |
0x03, |
RW |
1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Time delay |
|
0x0EDC |
3805 |
2 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |