Communication Status
The table lists the communication status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
|
0x02A0 |
673 |
0x02 |
R |
BOOL |
N |
Modbus RTU or PROFIBUS DP port – No communication |
|
0x02A1 |
674 |
0x02 |
R |
BOOL |
N |
HMI port – No communication |
|
0x02A4–0x02BF |
677–704 |
– |
– |
– |
– |
Reserved |