DOCA0355EN-01

Modbus RTU Network Characteristics

Overview

This section defines the characteristics of the Modbus RTU network over serial communication line. The Modbus RTU unit complies with the serial line specification. For information on serial line specification and implementation, see Serial Line Specification and Implementation Guide published on www.Modbus.org.

Standard Diagram

The standard diagram corresponds to the Modbus RTU specification on the www.Modbus.org site and in particular to the two-wire multidrop serial bus diagram.

The simplified diagram is as follows:

A End termination resistor
B Twisted cable
C Ground

Characteristics for Connection to Modbus RTU RS 485 Bus

The RS 485 standard allows variants with characteristics like:

  • Line terminator

  • Number of servers

  • Bus length

Characteristics

Value

Maximum number of stations

@Updated D4

32 stations, which is 31 servers

Type of trunk cable

Single, shielded, twisted pair cable, with 120 Ω characteristic impedance, and at least a third conductor

Maximum bus length

1000 m (3300 ft) at 19200 bps

Maximum length of tap-offs

  • 20 m (66 ft) for one tap-off

  • 40 m (131 ft) divided by the number of tap-offs on the multiple junction box

Line terminator

120 Ω resistor +/- 5% at both ends of the bus

Common polarity

Common polarity is connected to the protective ground in at least one point on the bus.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?