Under Frequency Protection
The table lists the under frequency protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0E49 |
3658 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0E4A |
3659 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%F* |
UINT16 |
90–100 |
94 |
Y |
Pickup |
|
0x0E4B |
3660 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
|
0x0E4C |
3661 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%F* |
UINT16 |
90–100 |
94 |
Y |
Alarm level |
|
0x0E4D |
3662 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E4E |
3663 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E4F |
3664 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |