DOCA0355EN-01

Motor Run Indicators

The table lists the motor run indicators for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0210

529

0x02

R

BOOL N

Motor forward running

0x0211

530

0x02

R

BOOL N

Motor reverse running

0x0212

531

0x02

R

BOOL N

Motor fast forward running

0x0213

532

0x02

R

BOOL N

Motor fast reverse running

0x0214

533

0x02

R

BOOL N

Motor running in star (forward)

0x0215

534

0x02

R

BOOL N

Motor running in delta (forward)

0x0216

535

0x02

R

BOOL N

Motor running in star (reverse)

0x0217

536

0x02

R

BOOL N

Motor running in delta (reverse)

0x0218

537

0x02

R

BOOL N

Motor in star-delta changeover (forward)

0x0219

538

0x02

R

BOOL N

Motor in star-delta changeover (reverse)

0x021A

539

0x02

R

BOOL N

Interlocking time active 

0x021B

540

0x02

R

BOOL N

Change-over pause active

0x021C–0x021F

541–544

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?