Trip Logs
Description
The last 20 encountered trips are recorded by the LTMT main unit. Each trip log is composed of 32 registers.
A read request of 32xn registers is necessary to read the last n trip logs, where 32 is the number of registers for each trip log.
The order and the description of the registers for trip log 1 are valid for the other trip logs.
| Address | Register | Description |
|---|---|---|
|
0x1770 |
6001–6032 |
Trip log 1 (most recent log) |
|
0x1790 |
6033–6064 |
Trip log 2 |
|
0x17B0 |
6065–6096 |
Trip log 3 |
|
0x17D0 |
6097–6128 |
Trip log 4 |
|
0x17F0 |
6129–6160 |
Trip log 5 |
|
0x1810 |
6161–6192 |
Trip log 6 |
|
0x1830 |
6193–6224 |
Trip log 7 |
|
0x1850 |
6225–6256 |
Trip log 8 |
|
0x1870 |
6257–6288 |
Trip log 9 |
|
0x1890 |
6289–6320 |
Trip log 10 |
|
0x18B0 |
6321–6352 |
Trip log 11 |
|
0x18D0 |
6353–6384 |
Trip log 12 |
|
0x18F0 |
6385–6416 |
Trip log 13 |
|
0x1910 |
6417–6448 |
Trip log 14 |
|
0x1930 |
6449–6480 |
Trip log 15 |
|
0x1950 |
6481–6512 |
Trip log 16 |
|
0x1970 |
6513–6544 |
Trip log 17 |
|
0x1990 |
6545–6576 |
Trip log 18 |
|
0x19B0 |
6577–6608 |
Trip log 19 |
|
0x19D0 |
6609–6640 |
Trip log 20 |
Trip Log 1 Registers
The table lists the registers for the trip log 1.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
| 0x1770 |
6001 |
4 |
0x03 |
R |
– |
– |
UINT16 |
Y |
|
| 0x1774 |
6005 |
1 |
0x03 |
R |
– |
– |
UINT16 |
Y |
|
| 0x1775 |
6006 |
1 |
0x03 |
R |
1 |
% |
UINT16 |
Y |
Thermal memory |
| 0x1776 |
6007 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
Y |
L1 RMS current |
| 0x1778 |
6009 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
Y |
L2 RMS current |
| 0x177A |
6011 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
Y |
L3 RMS current |
| 0x177C |
6013 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
Y |
Calculated ground current |
| 0x177E |
6015 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
Y |
Measured ground current |
| 0x1780 |
6017 |
1 |
0x03 |
R |
0.01 |
% |
UINT16 |
Y |
Current imbalance |
| 0x1781 |
6018 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
Y |
Current phase sequence |
| 0x1782 |
6019 |
1 |
0x03 |
R |
0.1 |
V |
UINT16 |
Y |
L1-L2 RMS voltage |
| 0x1783 |
6020 |
1 |
0x03 |
R |
0.1 |
V |
UINT16 |
Y |
L2-L3 RMS voltage |
| 0x1784 |
6021 |
1 |
0x03 |
R |
0.1 |
V |
UINT16 |
Y |
L3-L1 RMS voltage |
| 0x1785 |
6022 |
1 |
0x03 |
R |
0.01 |
% |
UINT16 |
Y |
Voltage imbalance |
| 0x1787 |
6023 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
Y |
Voltage phase sequence |
| 0x1787 |
6024 |
1 |
0x03 |
R |
0.01 |
Hz |
UINT16 |
Y |
System frequency |
| 0x1788 |
6025 |
1 |
0x03 |
R |
– |
– |
UINT16 |
Y |
MSB: System PF LSB: Motor status |
| 0x1789 |
6026 |
1 |
0x03 |
R |
0.1 |
– |
UINT16 |
Y |
MSB: L1 current THD LSB: L2 current THD |
| 0x178A |
6027 |
1 |
0x03 |
R |
0.1 |
– |
UINT16 |
Y |
MSB: L3 current THD LSB: L1 voltage THD |
| 0x178B |
6028 |
1 |
0x03 |
R |
0.1 |
– |
UINT16 |
Y |
MSB: L2 voltage THD LSB: L3 voltage THD |
| 0x178C |
6029 |
2 |
0x03 |
R |
0.001 |
– |
UINT32 |
Y |
Total active power |
| 0x178E |
6031 |
2 |
– |
– |
– |
– |
– |
– |
Reserved |