Interlock Protection Status
Interlock Protection Alarm Status
The table lists the interlock protection alarm status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
|
0x0160 |
353 |
0x02 |
R |
BOOL | N |
Interlock 1 alarm |
|
0x0161 |
354 |
0x02 |
R |
BOOL | N |
Interlock 2 alarm |
|
0x0162 |
355 |
0x02 |
R |
BOOL | N |
Interlock 3 alarm |
|
0x0163 |
356 |
0x02 |
R |
BOOL | N |
Interlock 4 alarm |
|
0x0164 |
357 |
0x02 |
R |
BOOL | N |
Interlock 5 alarm |
|
0x0165 |
358 |
0x02 |
R |
BOOL | N |
Interlock 6 alarm |
|
0x0166 |
359 |
0x02 |
R |
BOOL | N |
Interlock 7 alarm |
|
0x0167 |
360 |
0x02 |
R |
BOOL | N |
Interlock 8 alarm |
|
0x0168 |
361 |
0x02 |
R |
BOOL | N |
Interlock 9 alarm |
|
0x0169 |
362 |
0x02 |
R |
BOOL | N |
Interlock 10 alarm |
|
0x016A |
363 |
0x02 |
R |
BOOL | N |
Interlock 11 alarm |
|
0x016B |
364 |
0x02 |
R |
BOOL | N |
Interlock 12 alarm |
|
0x016C–0x016F |
365–368 |
– |
– |
– |
– |
Reserved |
Interlock Protection Pickup Status
The table lists the interlock protection pickup status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
|
0x0170 |
369 |
0x02 |
R |
BOOL | N |
Interlock 1 pickup |
|
0x0171 |
370 |
0x02 |
R |
BOOL | N |
Interlock 2 pickup |
|
0x0172 |
371 |
0x02 |
R |
BOOL | N |
Interlock 3 pickup |
|
0x0173 |
372 |
0x02 |
R |
BOOL | N |
Interlock 4 pickup |
|
0x0174 |
373 |
0x02 |
R |
BOOL | N |
Interlock 5 pickup |
|
0x0175 |
374 |
0x02 |
R |
BOOL | N |
Interlock 6 pickup |
|
0x0176 |
375 |
0x02 |
R |
BOOL | N |
Interlock 7 pickup |
|
0x0177 |
376 |
0x02 |
R |
BOOL | N |
Interlock 8 pickup |
|
0x0178 |
377 |
0x02 |
R |
BOOL | N |
Interlock 9 pickup |
|
0x0179 |
378 |
0x02 |
R |
BOOL | N |
Interlock 10 pickup |
|
0x017A |
379 |
0x02 |
R |
BOOL | N |
Interlock 11 pickup |
|
0x017B |
380 |
0x02 |
R |
BOOL | N |
Interlock 12 pickup |
|
0x017C–0x017F |
381–384 |
– |
– |
– |
– |
Reserved |
Interlock Protection Trip Status
The table lists the interlock protection trip status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
|
0x0180 |
385 |
0x02 |
R |
BOOL | N |
Interlock 1 trip |
|
0x0181 |
386 |
0x02 |
R |
BOOL | N |
Interlock 2 trip |
|
0x0182 |
387 |
0x02 |
R |
BOOL | N |
Interlock 3 trip |
|
0x0183 |
388 |
0x02 |
R |
BOOL | N |
Interlock 4 trip |
|
0x0184 |
389 |
0x02 |
R |
BOOL | N |
Interlock 5 trip |
|
0x0185 |
390 |
0x02 |
R |
BOOL | N |
Interlock 6 trip |
|
0x0186 |
391 |
0x02 |
R |
BOOL | N |
Interlock 7 trip |
|
0x0187 |
392 |
0x02 |
R |
BOOL | N |
Interlock 8 trip |
|
0x0188 |
393 |
0x02 |
R |
BOOL | N |
Interlock 9 trip |
|
0x0189 |
394 |
0x02 |
R |
BOOL | N |
Interlock 10 trip |
|
0x018A |
395 |
0x02 |
R |
BOOL | N |
Interlock 11 trip |
|
0x018B |
396 |
0x02 |
R |
BOOL | N |
Interlock 12 trip |
|
0x018C–0x018F |
397–400 |
– |
– |
– |
– |
Reserved |