LTMT Main Unit with Modbus RTU Protocol
Overview
The LTMT main unit with Modbus RTU protocol is equipped with two Modbus RTU communication connector types on the front face:
-
Plug-in 4-terminal connector
-
RJ45 port for HMI connection
The communication connectors follow the Modbus RTU interoperability standards. The use of the Modbus RTU 4-terminal connector is recommended. It allows daisy chain and point-to-point connection. The HMI port allows only point-to-point connection.
-
Terminal connection port
-
HMI port
Description
|
A |
Digital input terminals |
| B |
RJ45 port for expansion unit connection |
| C |
RJ45 port for HMI connection or Modbus RTU communication |
| D | Modbus RTU communication open-style connector |
|
E |
Temperature input terminal |
| F |
Power supply terminal |
| G |
QR code to product information page |
| H |
Test/Reset button |
| I | Status LEDs |
| J |
Digital output terminals |