Permissive Commands Status
The table lists the permissive commands status for the Modbus RTU communication.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
| 0x0220 |
545 |
0x02 |
R |
BOOL | N |
Status - Permissive Command 1 |
| 0x0221 |
546 |
0x02 |
R |
BOOL | N |
Status - Permissive Command 2 |
| 0x0222 |
547 |
0x02 |
R |
BOOL | N |
Status - Permissive Command 3 |
| 0x0223 |
548 |
0x02 |
R |
BOOL | N |
Status - Permissive Command 4 |
| 0x0224 |
549 |
0x02 |
R |
BOOL | N |
Status - Permissive Command 5 |
| 0x0225 |
550 |
0x02 |
R |
BOOL | N |
Status - Permissive Command 6 |
| 0x0226 |
551 |
0x02 |
R |
BOOL | N |
Status - Permissive Command 7 |
| 0x0227 |
552 |
0x02 |
R |
BOOL | N |
Status - Permissive Command 8 |
| 0x0228–0x023F |
553–576 |
– |
– |
– |
– |
Reserved |