LTMT Main Unit Device Internal Error Detection
The table lists the different device internal error detection setting of LTMT main unit.
|
Address |
Register |
Function code |
RW |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|
|
0x0260 |
609 |
0x02 |
R |
BOOL | N |
Sensor module communication error detected |
|
0x0261 |
610 |
0x02 |
R |
BOOL | N |
Expansion unit communication error detected |
|
0x0262 |
611 |
0x02 |
R |
BOOL | N |
Reserved |
|
0x0263 |
612 |
0x02 |
R |
BOOL | N |
EEPROM interface error detected |
|
0x0264 |
613 |
0x02 |
R |
BOOL | N |
EEPROM checksum error detected |
|
0x0265 |
614 |
0x02 |
R |
BOOL | N |
Configuration error detected |
|
0x0266 |
615 |
0x02 |
R |
BOOL | N |
PROFIBUS DP interface error detected |
|
0x0267 |
616 |
0x02 |
R |
BOOL | N |
Internal temperature major error detected |
|
0x0268 |
617 |
0x02 |
R |
BOOL | N |
Watchdog timeout detected |
|
0x0269 |
618–620 |
0x02 |
R |
BOOL | N |
Reserved |
|
0x026C |
621 |
0x02 |
R |
BOOL | N |
Energy register overflow |
|
0x026D |
622 |
0x02 |
R |
BOOL | N |
Error detected during LTMT expansion module initialization |
|
0x026E |
623 |
0x02 |
R |
BOOL | N |
Reserved |
|
0x026F |
624 |
0x02 |
R |
BOOL | N |
Write Pub Key failure |
|
0x026G–0x027F |
625–640 |
0x02 |
R |
BOOL | N |
Reserved |