DOCA0355EN-01

Definite Time Overcurrent Protection

The table lists the definite time overcurrent protection for the Modbus RTU communication.

Address

Register

No.

Function code

RW

X

Unit

Type

Range

Default value

Svd

Description

0x0DCA

3531

1

0x03,
0x06,
0x10

RW

1

UINT16

  • 0: Disable

  • 1: Alarm

  • 2: Trip

  • 3: Alarm + Trip

2

Y

Function setting

0x0DCB

3532

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

20–1000
(step 1)

110

Y

Pickup

0x0DCC

3533

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

300

Y

Time delay during motor start (TpS)

0x0DCD

3534

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

1–60000
(step 1)

200

Y

Time delay during motor run (TpR)

0x0DCE

3535

1

0x03,
0x06,
0x10

RW

1

%IFLC

UINT16

20–1000
(step 1)

110

Y

Alarm level

0x0DCF

3536

1

0x03,
0x06,
0x10

RW

1

BITMAP

  • Bit 0: Reset key

  • Bit 1: DI
  • Bit 2: Communication
  • Bit 3: Auto

3

Y

Reset mode

0x0DD0

3537

1

0x03,
0x06,
0x10

RW

0.1

s

UINT16

0–60000
(step 1)

0

Y

Auto-Reset delay

0x0DD1

3538

1

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?