Short Time Overcurrent Protection
The table lists the short time overcurrent protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0DD9 |
3546 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0DDA |
3547 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
100–1000 |
100 |
Y |
Pickup |
|
0x0DDB |
3548 |
1 |
0x03, 0x06, 0x10 |
RW |
0.01 |
s |
UINT16 |
5–1000 |
5 |
Y |
Time delay |
|
0x0DDC |
3549 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
%IFLC |
UINT16 |
100–1000 |
100 |
Y |
Alarm level |
|
0x0DDD |
3550 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0DDE |
3551 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0DDF |
3552 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |