Digital Input Interlock Protection Settings
Description
Each digital input interlock protection settings are made up of five registers. The order and the description of the settings for digital input 1 interlock are valid for the other digital inputs.
|
Address |
Register |
RW |
Function code |
Description |
|---|---|---|---|---|
|
0x0F23–0x0F27 |
3876–3880 |
RW |
0x03,0x06,0x10 |
Digital input 1 interlock protection settings |
|
0x0F28–0x0F2C |
3881–3885 |
RW |
0x03,0x06,0x10 |
Digital input 2 interlock protection settings |
|
0x0F2D–0x0F31 |
3886–3890 |
RW |
0x03,0x06,0x10 |
Digital input 3 interlock protection settings |
|
0x0F32–0x0F36 |
3891–3895 |
RW |
0x03,0x06,0x10 |
Digital input 4 interlock protection settings |
|
0x0F37–0x0F3B |
3896–3900 |
RW |
0x03,0x06,0x10 |
Digital input 5 interlock protection settings |
| 0x0F3C–0x0F40 |
3901–3905 |
RW |
0x03,0x06,0x10 |
Digital input 6 interlock protection settings |
|
0x0F41–0x0F45 |
3906–3910 |
RW |
0x03,0x06,0x10 |
Digital input 7 interlock protection settings |
|
0x0F46–0x0F4A |
3911–3915 |
RW |
0x03,0x06,0x10 |
Digital input 8 interlock protection settings |
|
0x0F4B–0x0F4F |
3916–3920 |
RW |
0x03,0x06,0x10 |
Digital input 9 interlock protection settings |
|
0x0F50–0x0F54 |
3921–3925 |
RW |
0x03,0x06,0x10 |
Digital input 10 interlock protection settings |
|
0x0F55–0x0F59 |
3926–3930 |
RW |
0x03,0x06,0x10 |
Digital input 11 interlock protection settings |
|
0x0F5A–0x0F5E |
3931–3935 |
RW |
0x03,0x06,0x10 |
Digital input 12 interlock protection settings |
Digital Input 1 Interlock Protection Settings
The table lists the registers for the digital input interlock protection settings.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0F23 |
3876 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0F24 |
3877 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
0–6000 |
0 |
Y |
Time delay |
|
0x0F25 |
3878 |
1 |
0x03, |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0F26 |
3879 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
0–6000 |
0 |
Y |
Auto-Reset delay |
|
0x0F27 |
3880 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |