DOCA0355EN-01

Protection Function Status

Protection Alarm Status

The table lists the protection alarm status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0100

257

0x02

R

BOOL N

Thermal overload alarm

0x0101

258

0x02

R

BOOL N

Locked rotor alarm

0x0102

259

0x02

R

BOOL N

Stalled rotor alarm

0x0103

260

0x02

R

BOOL N

Definite time overcurrent alarm

0x0104

261

0x02

R

BOOL N

Normal inverse overcurrent alarm

0x0105

262

0x02

R

BOOL N

Short time overcurrent alarm

0x0106

263

0x02

R

BOOL N

Calculated ground current alarm

0x0107

264

0x02

R

BOOL N

Measured ground current alarm

0x0108

265

0x02

R

BOOL N

Phase under current alarm

0x0109

266

0x02

R

BOOL N

Current imbalance alarm

0x010A

267

0x02

R

BOOL N

Current phase loss alarm

0x010B

268

0x02

R

BOOL N

Current phase reversal alarm

0x010C

269

0x02

R

BOOL N

Phase under voltage alarm

0x010D

270

0x02

R

BOOL N

Phase over voltage alarm

0x010E

271

0x02

R

BOOL N

Voltage phase loss alarm

0x010F

272

0x02

R

BOOL N

Voltage imbalance alarm

0x0110

273

0x02

R

BOOL N

Voltage phase reversal alarm

0x0111

274

0x02

R

BOOL N

Under frequency alarm

0x0112

275

0x02

R

BOOL N

Over frequency alarm

0x0113

276

0x02

R

BOOL N

Reserved

0x0114

277

0x02

R

BOOL N

Communication loss alarm

0x0115

278

0x02

R

BOOL N

Over temperature alarm

0x0116

279

0x02

R

BOOL N

Under power alarm

0x0117

280

0x02

R

BOOL N

Over power alarm

0x0118

281

0x02

R

BOOL N

Under power factor alarm

0x0119

282

–

–

–

–

Reserved

0x011A

283

0x02

R

BOOL N

Device internal temperature alarm

0x011B

284

0x02

R

BOOL N

HMI communication loss alarm

0x011C–0x011F

285–288

–

–

–

–

Reserved

Protection Pickup Status

The table lists the protection pickup status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0120

289

0x02

R

BOOL N

Thermal overload pickup

0x0121

290

0x02

R

BOOL N

Locked rotor pickup

0x0122

291

0x02

R

BOOL N

Stalled rotor pickup

0x0123

292

0x02

R

BOOL N

Definite time overcurrent pickup

0x0124

293

0x02

R

BOOL N

Normal inverse overcurrent pickup

0x0125

294

0x02

R

BOOL N

Short time overcurrent pickup

0x0126

295

0x02

R

BOOL N

Calculated ground current pickup

0x0127

296

0x02

R

BOOL N

Measured ground current pickup

0x0128

297

0x02

R

BOOL N

Phase under current pickup

0x0129

298

0x02

R

BOOL N

Current imbalance pickup

0x012A

299

0x02

R

BOOL N

Current phase loss pickup

0x012B

300

0x02

R

BOOL N

Current phase reversal pickup

0x012C

301

0x02

R

BOOL N

Phase under voltage pickup

0x012D

302

0x02

R

BOOL N

Phase over voltage pickup

0x012E

303

0x02

R

BOOL N

Voltage phase loss pickup

0x012F

304

0x02

R

BOOL N

Voltage imbalance pickup

0x0130

305

0x02

R

BOOL N

Voltage phase reversal pickup

0x0131

306

0x02

R

BOOL N

Under frequency pickup

0x0132

307

0x02

R

BOOL N

Over frequency pickup

0x0133

308

0x02

R

BOOL N

Excessive start time pickup

0x0134

309

0x02

R

BOOL N

Communication loss pickup

0x0135

310

0x02

R

BOOL N

Over temperature pickup

0x0136

311

0x02

R

BOOL N

Under power pickup

0x0137

312

0x02

R

BOOL N

Over power pickup

0x0138

313

0x02

R

BOOL N

Under power factor pickup

0x0139

314

–

–

–

–

Reserved

0x013A

315

0x02

R

BOOL N

Device internal pickup

0x013B

316

0x02

R

BOOL N

HMI communication loss pickup

0x013C–0x013F

317–320

–

–

–

–

Reserved

Protection Trip Status

The table lists the protection trip status for the Modbus RTU communication.

Address

Register

Function code

RW

Type

Svd

Description

0x0140

321

0x02

R

BOOL N

Thermal overload trip

0x0141

322

0x02

R

BOOL N

Locked rotor trip

0x0142

323

0x02

R

BOOL N

Stalled rotor trip

0x0143

324

0x02

R

BOOL N

Definite time overcurrent trip

0x0144

325

0x02

R

BOOL N

Normal inverse overcurrent trip

0x0145

326

0x02

R

BOOL N

Short time overcurrent trip

0x0146

327

0x02

R

BOOL N

Calculated ground current trip

0x0147

328

0x02

R

BOOL N

Measured ground current trip

0x0148

329

0x02

R

BOOL N

Phase under current trip

0x0149

330

0x02

R

BOOL N

Current imbalance trip

0x014A

331

0x02

R

BOOL N

Current phase loss trip

0x014B

332

0x02

R

BOOL N

Current phase reversal trip

0x014C

333

0x02

R

BOOL N

Phase under voltage trip

0x014D

334

0x02

R

BOOL N

Phase over voltage trip

0x014E

335

0x02

R

BOOL N

Voltage phase loss trip

0x014F

336

0x02

R

BOOL N

Voltage imbalance trip

0x0150

337

0x02

R

BOOL N

Voltage phase reversal trip

0x0151

338

0x02

R

BOOL N

Under frequency trip

0x0152

339

0x02

R

BOOL N

Over frequency trip

0x0153

340

0x02

R

BOOL N

Excessive start time trip

0x0154

341

0x02

R

BOOL N

Communication loss trip

0x0155

342

0x02

R

BOOL N

Over temperature trip

0x0156

343

0x02

R

BOOL N

Under power trip

0x0157

344

0x02

R

BOOL N

Over power trip

0x0158

345

0x02

R

BOOL N

Under power factor trip

0x0159

346

0x02

R

BOOL N

Reserved

0x015A

347

0x02

R

BOOL N

Device internal trip

0x015B

348

0x02

R

BOOL N

HMI communication loss trip

0x015C–0x015F

349–352

0x02

R

BOOL N

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?