Metering Data
The table lists the metering data for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x157C |
5501 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
N |
L1 RMS current |
|
0x157E |
5503 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
N |
L2 RMS current |
|
0x1580 |
5505 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
N |
L3 RMS current |
|
0x1582 |
5507 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
N |
Measured ground current |
|
0x1584 |
5509 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
N |
Calculated ground current |
|
0x1586 |
5511 |
2 |
0x03 |
R |
0.001 |
A |
UINT32 |
N |
Average current |
|
0x1588 |
5513 |
1 |
0x03 |
R |
0.01 |
% |
UINT16 |
N |
Current imbalance |
|
0x1589 |
5514 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Current phase sequence
|
|
0x158A |
5515 |
2 |
0x03 |
R |
0.1 |
V |
UINT32 |
N |
For single phase, L1–N RMS voltage For three phase, L1–L2 RMS voltage |
|
0x158C |
5517 |
2 |
0x03 |
R |
0.1 |
V |
UINT32 |
N |
L2–L3 RMS voltage |
|
0x158E |
5519 |
2 |
0x03 |
R |
0.1 |
V |
UINT32 |
N |
L3–L1 RMS voltage |
|
0x1590 |
5521 |
2 |
0x03 |
R |
0.1 |
V |
UINT32 |
N |
Average voltage |
|
0x1592 |
5523 |
1 |
0x03 |
R |
0.01 |
% |
UINT16 |
N |
Voltage imbalance |
|
0x1593 |
5524 |
1 |
0x03 |
R |
1 |
– |
UINT16 |
N |
Voltage phase sequence
|
|
0x1594 |
5525 |
1 |
0x03 |
R |
0.01 |
Hz |
UINT16 |
N |
System frequency |
|
0x1595 |
5526 |
1 |
0x03 |
R |
0.01 |
– |
UINT16 |
N |
System power factor |
|
0x1596 |
5527 |
2 |
0x03 |
R |
0.001 |
kW |
UINT32 |
N |
Total active power |
|
0x1598 |
5529 |
2 |
0x03 |
R |
0.001 |
kvar |
UINT32 |
N |
Total reactive power |
|
0x159A |
5531 |
2 |
0x03 |
R |
0.001 |
kVA |
UINT32 |
N |
Total apparent power |
|
0x159C |
5533 |
4 |
0x03 |
R |
0.001 |
kWh |
UINT64 |
Y |
Total active energy |
|
0x15A0 |
5537 |
4 |
0x03 |
R |
0.001 |
kvarh |
UINT64 |
Y |
Total reactive energy |
|
0x15A4 |
5541 |
4 |
0x03 |
R |
0.001 |
kVAh |
UINT64 |
Y |
Total apparent energy |
|
0x15A8 |
5545 |
1 |
0x03 |
R |
1 |
% |
UINT16 |
N |
L1 Current THD |
|
0x15A9 |
5546 |
1 |
0x03 |
R |
1 |
% |
UINT16 |
N |
L2 Current THD |
|
0x15AA |
5547 |
1 |
0x03 |
R |
1 |
% |
UINT16 |
N |
L3 Current THD |
|
0x15AB |
5548 |
1 |
0x03 |
R |
1 |
% |
UINT16 |
N |
For single phase, L1–N Voltage THD For three phase, L1–L2 Voltage THD |
|
0x15AC |
5549 |
1 |
0x03 |
R |
1 |
% |
UINT16 |
N |
L2–L3 Voltage THD |
|
0x15AD |
5550 |
1 |
0x03 |
R |
1 |
% |
UINT16 |
N |
L3–L1 Voltage THD |
|
0x15AE |
5551 |
1 |
0x03 |
R |
0.1 |
°C or F |
UINT16 |
N |
Temperature measured by PT100 sensor* |
|
0x15AF |
5552 |
1 |
0x03 |
R |
1 |
Ω |
UINT16 |
N |
Temperature measured by binary PTC sensor |
|
0x15B0 |
5553 - 5556 |
3 |
– |
– |
– |
– |
– |
– |
Reserved |