HMI Communication Loss
The table lists the HMI communication loss for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0EDE |
3807 |
1 |
0x03, |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0EDF |
3808 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
– |
10 |
Y |
Time delay |
|
0x0EE0 |
3809 |
1 |
0x03, – |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0EE1 |
3810 |
1 |
0x03, |
RW |
0.1 |
s |
UINT16 |
– |
0 |
Y |
Auto-Reset delay |
|
0x0EE2 |
3811 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |