Under Power Factor Protection
The table lists the under power factor protection for the Modbus RTU communication.
|
Address |
Register |
No. |
Function code |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|---|---|
|
0x0E65 |
3686 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0E66 |
3687 |
1 |
0x03, 0x06, 0x10 |
RW |
0.10 |
PF |
UINT16 |
40–100 |
60 |
Y |
Pickup |
|
0x0E67 |
3688 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
1–60000 |
1 |
Y |
Time delay |
|
0x0E68 |
3689 |
1 |
0x03, 0x06, 0x10 |
RW |
0.10 |
PF |
UINT16 |
40–100 |
60 |
Y |
Alarm level |
|
0x0E69 |
3690 |
1 |
0x03, 0x06, 0x10 |
RW |
1 |
– |
BITMAP |
|
3 |
Y |
Reset mode |
|
0x0E6A |
3691 |
1 |
0x03, 0x06, 0x10 |
RW |
0.1 |
s |
UINT16 |
0–60000 |
0 |
Y |
Auto-Reset delay |
|
0x0E6B |
3692 |
1 |
– |
– |
– |
– |
– |
– |
– |
– |
Reserved |